Skip to main content
Associate III
December 22, 2024
Question

Motor Control Workbench: Regarding the working & modification of generated code

Hi Sir, I have steval spin3202 evaluation board for an application of bldc motor application. I have generated code using Motor Control Workbench, initally for testing i tested it out using Motor Pilot it was working as expected using Start and stop command using the interface, but i want little modification such that i dont want to control it using motor pilot interface for that, I turn off the UART button in the selection and again flash the code to run the motor but for the running of the motor i need to press the reset button after that i can control the motor usign potentiometer, i also dont want to use user button.

Following thing i need to do in the code,

1) When i power the board it  should start the motor, i.e i don't want to press the reset button manually for the starting of the motor as for my application i also don't want user button to start the motor.

2) In my application if the Source current is greater than 7A it should turn off the motor but in the code i have selected the max of 50A in the current limit i.e when i apply the setting of 50A and run the motor the current drawing from the souce was 3A but as the requirement was to set the current limit how to set it. As earlier i have set to 10A in the motor control workbench but the motor was not working.

3) For Over and Under voltage if i have set undervoltage to 9V it is also working at 8.90V and if i have set the over voltage to 16V the motor is not working at 15.3V. How to set  the floating values for it.

4)As there might be a situation where some error is generated like overvoltage, undervoltage, overcurrent etc, i need to modify code such that it will wait for 30seconds and try to run the motor if all the error is clear or else again it will wait for 30 second.

5) If i want to integrate the LIN Signal as input then how to do it, i.e  as currently adc is input signal now LIN is the input signal to control the motor

6) If the board is running for long time like 3-6 months what will be the characteristics of the board regarding temperature of the pcb and health of the component, is there any safety measure for component regarding the increase of the temperature especially for STSPIN3202F0A.

Thankyou sir for reading such a long problem statement, but as i need to elaborate my problem for understanding it in precise way so that the solution can be more precise The solution of it will help me a lot.

This topic has been closed for replies.

3 replies

Gael A
ST Employee
January 6, 2025

Hello Shubham08,

Unfortunately, we cannot provide extended support on purely applicative issues. You can find a set of APIs located in the mc_api.c file. They are meant to be used to develop your application according to your needs in the main.c file.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.
Shubham08Author
Associate III
January 13, 2025

Yes sir, I will look for mc_api.c file and get back if there is any doubt in it

Shubham08Author
Associate III
April 2, 2025

Recently through debugging the uart issue was solved in custom board and i was able to connect to motor pilot, but found the issue that it was starting with undervoltage, getting error like speed feedback error and overcurrent error although there was no load in motor after pressing the reset 2-3 times the motor was running smoothly.

I need help in software part as below

1) how to set the parameters in motor controller because i have tried, but as i have set under voltage at 9V and giving the supply of 12V then also it is showing undervoltage, setting the speed configuration in sensorless startup as shown in the image it is not properly set and not getting how to calculate the parameters.

Shubham08_0-1743594793031.png

 

2)I have set the parameter for overcurrent to 50A but then also it showing error when motor is under no load.

3)In the code how to add such that if the the input supply current is greater than X A then the motor controller should top and for any other error it should wait for 15sec and then clear the error and again try to run the motor.

 

sir don't suggest some file or API like mc_api and all because previously also getting the same response and the problem is not solved Give a code snippet to add and solve the problem