Skip to main content
Mathan Raja
Associate III
September 7, 2021
Question

Motor Control workbench

Hi,

I am using NUCLEO-F303RE,

I have purchased a power board (IPM evaluation board EVALM13645ATOBO1) from Digikey.

  1. In the Motor control workbench, I didn't find above mentioned power board part no. so, can you tell me, which one I need to select in the drop-down list of power board custom board or else?
  2. In current sensing & Bus voltage sensing, the below-shown circuit value,

Is automatically calculated? or Is the user needs to configure this value?

If yes, where or how to find/check these values? 0693W00000DmMqMQAV.png0693W00000DmMqCQAV.png 3. is it possible to change the board details once it is selected.

0693W00000DmN1UQAV.png 

This topic has been closed for replies.

2 replies

Laurent Ca...
Senior III
September 15, 2021

Dear @Mathan Raja​ 

We are sorry but we only support ST power boards.

I don't know your board but I guess you can design your own based on a similar existing board.

Best regards

Mathan Raja
Associate III
September 20, 2021

Hi Laurent,

which ST power board is the same as EVALM13645ATOBO1 ( Equivalent)?

How can I use Motor Profiler software (for finding motor parameters), with the Nucleo-F303RE & EVALM13645ATOBO1 boards?

Thanks