Skip to main content
Visitor II
Jun 17, 2025 11:10 AM UTC
Question

motor control using cubeide for hss86 driver

I tried to rotate the nema34 stepper motor through hss86 motor driver using the stm32 G474RE. I configured the pins as follow:  Pul - connected to Tim 3_CH 1(PA6) , Dir - connected to GPIO OUTPUT_B_10 , Ena - connected to GPIO OUTPUT_D_2 and all the positive terminals to the 5V battery and grounded it to the stm32 pin(GND) . I also generated the output pulse and upload my code to the stm 32 without any error, Although the motor is not rotating. Is there any specific code I have to write  beyond the PWM generation code.  

This topic has been closed for replies.

2 replies

GMA
ST Technical Moderator
Jul 24, 2025 3:06 PM UTC

Hello @Smritha,

As HSS86 is not an ST product, I can only recommend using an oscilloscope to ensure that the TIMER and GPIO outputs are generated as expected.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Chris21
Associate II
Jul 24, 2025 4:29 PM UTC

It looks like the HSS86 is expecting 5 volts or more, STM32 GPIOs are not at the level, generally.

.