Skip to main content
Visitor II
Feb 18, 2026 4:52 AM UTC
Question

Motor Control SDK support H723ZG

Hello, 

We want to use the STMH723ZG with the Motor Control SDK. To do this I cannot find the .json file support for the board in the motor control workbench. Could I use another .json file from one of the fully-supported boards like the H745? 

Also, we are using custom power electronics + motor setup so to my knowledge our board has sensors it outputs to the stm + it takes a pwm 3-phase input from the stm to spin the motors. What all info do I need and what process do I follow to get a project built for this setup with the motor control SDK.

1 reply

GMA
ST Technical Moderator
Mar 3, 2026 3:53 PM UTC

Hello @hmantha,

As stated in the MCSDK release note, two microcontrollers are supported for the STM32H7xx family: STM32H745ZI and STM32H755ZITx.

The MCSDK toolkit provides the Motor Control Board Designer tool, located in the MC_SDK_x.x.x\Utilities\PC_Software\STMCBD directory, to describe a custom board for MC Workbench.
In the MC Board Designer tool, select the About button to access documentation.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA