Skip to main content
Gigi
ST Employee
January 23, 2014
Question

Motor control news from STMicroelectronics - Jan 2014

Posted on January 23, 2014 at 16:00

http://links.st-microelectronics.mkt5947.com/ctt?kn=25&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

http://links.st-microelectronics.mkt5947.com/ctt?kn=22&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

http://links.st-microelectronics.mkt5947.com/ctt?kn=4&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

ST�s motor control software development kit provides all you need for the development of your motor control application based on the STM32 F0, F1, F2, F4 and now F3 (release v3.4) MCUs. It supports up to two PMSMs using any combination of current reading topologies and speed/position sensors, including sensorless operation. Application development and optimization is facilitated by the PC based MC Workbench software. This GUI sets SDK parameters, real-time access to control variables including their display on a virtual oscilloscope.

http://links.st-microelectronics.mkt5947.com/ctt?kn=25&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

Gigi

#stsw-stm32100-pmsm-foc-sdk
This topic has been closed for replies.

12 replies

hassanbhutta91
Visitor II
December 12, 2014
Posted on December 12, 2014 at 17:11

Laurent Ca...
Senior III
June 21, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards