Question
Motor control and PMSM_FOC stm32-mat/target example not run on my stm32f429i-DISC1 .
I stay try to run this example on my board in PIL mode(i change project target to stm32.tlc instead the buildin stm32f302r_nucleo) , but i receive from sw4stm32 error for missing arm_math.h . I include the link to the file from the stm32cube repository, and after i have FPU error. when in the preprocessor i add " __FPU_PRESENT " the error go to arm_cos_f32....
How i can solve it? How i must setting the parameters in simulink or eclipse?:face_with_steam_from_nose: