Skip to main content
Associate
January 18, 2024
Solved

Missing files when generating profiler FW with MCSDK v6.2.1

Hi,

 

I am trying to generate profiler FW for my board (B-G431B-ESC1), 

I have checked the "Motor Profiler" checkbox and created the project for STM32CubeIDE.

 

In the "MCSDK_v6.2.1-Full\MotorControl\MCSDK\MCLib\Any\Src" I am missing 3 files:

mp_hall_tuning.c

mp_one_touch_tuning.c

mp_self_com_ctrl.c

I do see the corresponding .h files in "..\Inc"

I tried the same with MCSDK 6.2.0, same result.

 

Thanks,

 

Yoav

    This topic has been closed for replies.
    cedric H
    cedric HBest answer
    ST Technical Moderator
    January 19, 2024

    Hello @Wattever,

    Your link issue comes from the version of cubeIDE.

    From your installation path, I see that you are using version 1.12.1. 

    In order to be able to link with the profiler library you must have at least version 1.14.0.

    This requirement is specified in the release note.

    Regards

    Cedric

    5 replies

    Fabrice LOUBEYRE
    ST Employee
    January 18, 2024

    Hi, the files are not provided as source file but are embedded into libraries located into the libMP directory of the MCSDK package. As soon as you have generated a motor Profiler project, the lib containing the motor profiler algorithm will be present int your source directory.

    Best regards

    Fabrice

    WatteverAuthor
    Associate
    January 18, 2024

    Hi,

     

    Thanks for your reply.

     

    When I try to compile the code I get the following errors:

    ..MCSDK_v6.2.0-Full/MotorControl/libMP\libmp-IAR_ARMv7-M.a(mp_one_touch_tuning.o): unknown mandatory EABI object attribute 50

    c:\st\stm32cubeide_1.12.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe: failed to merge target specific data of file ../../MCSDK_v6.2.0-Full/MotorControl/libMP\libmp-IAR_ARMv7-M.a(mp_one_touch_tuning.o)


    MCSDK_v6.2.0-Full/MotorControl/libMP\libmp-IAR_ARMv7-M.a(mp_self_com_ctrl.o): unknown mandatory EABI object attribute 50

    c:\st\stm32cubeide_1.12.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe: failed to merge target specific data of file ../../MCSDK_v6.2.0-Full/MotorControl/libMP\libmp-IAR_ARMv7-M.a(mp_self_com_ctrl.o)


    MCSDK_v6.2.0-Full/MotorControl/libMP\libmp-IAR_ARMv7-M.a(mp_hall_tuning.o): unknown mandatory EABI object attribute 50
    c:\st\stm32cubeide_1.12.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe: failed to merge target specific data of file ../../MCSDK_v6.2.0-Full/MotorControl/libMP\libmp-IAR_ARMv7-M.a(mp_hall_tuning.o)

    Fabrice LOUBEYRE
    ST Employee
    January 18, 2024

    Hi,

    We manage the compilation and link of the generated project with the STM32CubeIde IDE tool. The project generated with the MCSDKWB tool generate a .project with all information required for the tool.

    The link is then executed with the following arm-none-eabi-gcc -o -Wl  command and not ld.exe.

    example of linker line execution with -Wl option for link with no ld command:

    arm-none-eabi-gcc -o "test_forum_6_2_0.elf" @"objects.list" -l:libmp-IAR_ARMv7-M.a -mcpu=cortex-m4 -T"test_forum_6_2_0\STM32CubeIDE\STM32G431CBUX_FLASH.ld" --specs=nosys.specs -Wl,-Map="test_forum_6_2_0.map" -Wl,--gc-sections -static -L../../MCSDK_v6.2.0-Full/MotorControl/libMP --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group

     

    Best regards

    Fabrice

    cedric H
    cedric HBest answer
    ST Technical Moderator
    January 19, 2024

    Hello @Wattever,

    Your link issue comes from the version of cubeIDE.

    From your installation path, I see that you are using version 1.12.1. 

    In order to be able to link with the profiler library you must have at least version 1.14.0.

    This requirement is specified in the release note.

    Regards

    Cedric

    WatteverAuthor
    Associate
    January 21, 2024

    Hi Cedric,

     

    Thank you, upgrade CubeIDE to  1.14.1 indeed solved the issue.

     

    B.R.

    Yoav