Question
MDSK5.4.8 CAN Communication Not working
- 1 reply
- 1275 views
hi.
I using MDSK 5.4.8 with NUCLEO F103RB / NUCLEO IMH07M1
The speed control operation was confirmed through the variable volume.
So now, I want to operate CAN 2.0A Communication
I already set CUBEMX pin & CAN setting.
Now, i just send message(tx test)
Development environment
=> X-NUCLEO-IHM07M1 Power input J2 ( 24V )
=> NUCELO-F103RB CN1(USB) - PC
1. X-NUCLEO-IHM07M1 Power input J2 ( 24V ) & NUCELO-F103RB CN1(USB) - PC
=> motor not working / CAN notworking
2. X-NUCLEO-IHM07M1 Power Off & NUCELO-F103RB CN1(USB) - PC
=> motor not working / CAN Working
I want to operation motor & can at the same time
How to??