Skip to main content
mkosu.2
Visitor II
January 12, 2023
Question

MCSDK 6.1 generated project for Steval-spin3201 board does not work in closed-loop operation mode.

  • January 12, 2023
  • 0 replies
  • 511 views

I have created ioc project using MCSDK 6.1 for steval-spin3201 board to control a BLDC motor in sensorless PLL mode and/or HALL sensor mode. I have used ST Cube MX to generate Cube IDE project files , build them and downloaded executable files to the board. I have used ST Pilot program to communicate with the board . I was able to start and stop the motor but I could not make the motor run at the speed that I have set. Motor actual speed oscillates in a very wide range around the value that I have specified. It seems to me , speed regulation ( closed loop operation) does not work .

This topic has been closed for replies.