Skip to main content
AShin.5
Associate II
May 19, 2022
Question

MCSDK 5.y.x 6-step firmware generation

Hello,

I have STEVAL-SPIN3204 board and a BLDC motor with hall sensor.

So, I try to generate a firmware with 6-step control and hall sensors.

ST Motor Control workbench (v5.y.4) generate the firmware.

But, the source code folder have not MCLib6Step folder that is the control library for 6step control.

Also, mc_tasks.c.h in src/inc folders do not use the 6-step control library inside MCLib6Step folder, but do the FOC control library inside MCLib folder.

How can I generate the firmware with 6 step control library.

Thanks.

AShin.

This topic has been closed for replies.

3 replies

AShin.5
AShin.5Author
Associate II
May 21, 2022

Nobody is there???

Plz help!!!

kelvin.wang
Associate II
May 23, 2022

For current version . MCSDK support only FOC. 6 step can only be generated by example project.

AShin.5
AShin.5Author
Associate II
May 23, 2022

Mr. Kelvin ****,

I did not know that.

Many thanks for good answer.

let me think for a while,

I need to decide whether the firmware is modified from an example or not.

Thanks a lot.

AShin