Skip to main content
GBeno
Visitor II
Apr 29, 2019 3:23 PM UTC
Question

MCSDK 5.3.3: code wont execute_ TIM1

Hi,

I'm developing an Motor application using F446RE and MCSKD on custom board and custom motor control project, but the program never reaches the user code while loop.

I generated the code with ST Motor Control Worbench with 5.2.0 Cube MX andFirmware package version V1.24.1. And Build that with TrueStudio.

I commented these lines so that the code turns and can communicate in uart with ST workbench:

HAL_NVIC_SetPriority(TIM1_BRK_TIM9_IRQn, 4, 1);

HAL_NVIC_EnableIRQ(TIM1_BRK_TIM9_IRQn);

I could test the rest of the code: it works. ADC reads the value of vbus

Do you have an idea to use the TIMER 1 ?

Thanks you !

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
Jun 22, 2021 8:36 AM UTC

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards