Visitor II
Oct 17, 2018 4:13 AM UTC
Question
MC workbench problem when project generation
- 1 reply
- 659 views
Hi ST ,
I use MC workbenck 5.2 to build a motor control project.
I select example project "STM32303E-EVAL-IHM045V1-Shinano-DUAL-DRIVE".
Use project generation function to build Keil MDK project, and everything is OK,
BUT, after modify some parameters, click generation->Update, and the MC workbenck program is halted like attached picture.
how to fix this problem ??
(i use single motor project ,"NUCLEO-F303RE-IPM10B-Shinano" , generate and update function is OK, only when i use dual motor project , always have update problem.... )