Skip to main content
Senior
July 11, 2024
Question

MC workbench generation has errors.

  • July 11, 2024
  • 3 replies
  • 896 views

hello, 

now i am trying to use MC workbench 6.3.0 to generate a simple design, but there are errors.

the log is like below:

dqsh06_0-1720684006324.pngdqsh06_1-1720684113794.pngdqsh06_2-1720684138769.png

what is worry with MC workbench?  please help. 

thanks.

This topic has been closed for replies.

3 replies

GMA
ST Technical Moderator
July 11, 2024

Hello @dqsh06,

The issue is already followed in this post.
As the project is fully generated, you can compile and use it.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
dqsh06Author
Senior
July 12, 2024

Hello GMA,

I have checked the post you mentioned, it seems the issue is still open, errors still occur.

but you said the project is fully generated, i can use it. so you mean the errors can be ignored , just use the codes, right?

i will try.

Thanks,

dqsh  

GMA
ST Technical Moderator
July 12, 2024

Hello @dqsh06,

Yes, issue is under investigation. Please ignore it for the moment and use generated project.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA