Skip to main content
magene
Senior
October 31, 2023
Solved

Low voltage, high power, low speed application

  • October 31, 2023
  • 6 replies
  • 2116 views

I just listened to the New STM32 Motor Control SDK update webinar.  It was very good but I have a question that didn't get answered.  Can you recommend a set of eval hardware and software for this app:

Motor: 3 phase BLDC

Voltage: 12VDC (or lower) minimum to 42VDC (or higher) maximum

Current: 10 amps continuous with peaks to 15 Amps for at least 10s of seconds.

It is a battery powered application so energy efficiency is important as is low speed control down to 10-20 RPM.  Encoders are fine but an encoderless solution would be great.

This topic has been closed for replies.
Best answer by FouadB

Hello,

Thank you for your interest in ST's webinar on the New STM32 Motor Control SDK update.

Based on your required functionality, the recommended hardware setup would be :

Control board - NUCLEO-G431RB and Power board - X-NUCLEO-IHM08M1 (rated current of 30A and rated voltage range of 10-48V).

Both sensor or sensorless FOC control can be configured via the MC Workbench6.2.

Best regards

6 replies

FouadB
FouadBBest answer
ST Employee
November 2, 2023

Hello,

Thank you for your interest in ST's webinar on the New STM32 Motor Control SDK update.

Based on your required functionality, the recommended hardware setup would be :

Control board - NUCLEO-G431RB and Power board - X-NUCLEO-IHM08M1 (rated current of 30A and rated voltage range of 10-48V).

Both sensor or sensorless FOC control can be configured via the MC Workbench6.2.

Best regards

If you agree with my answer, please accept it by clicking on 'Accept as solution'.""
magene
mageneAuthor
Senior
November 3, 2023

Excellent, thank you.

cedric H
ST Technical Moderator
November 3, 2023

Hello @magene 

IHM08M1 indeed matches your electrical requirements, but be careful, low speed control could not be achieved with sensor less algorithm on this board. HSO is not available on IHM08, but encoder is ok.

Regards

Cedric