Skip to main content
Associate II
Jan 9, 2026 4:30 PM UTC
Question

Low speed control algorithms with sensors

Hi - What is the best algorithm for a very low speed and low current application, <50 RPM and <1 Amp with a high resolution encoder (~4096 counts per revolution) on a 3 phase brushless motor? Do the HSO or ZEST algorithms provide any advantage over the standard FOC algorithm when running with an encoder like this? I'm assuming the FOC algorithm is better than the 6 step algorithm, is that correct? Are there any other tips for this application?

 

Thanks

8 replies

Senior III
Jan 10, 2026 9:20 AM UTC

Yes FOC is better than 6 step algorithm. 

federico.rodighiero87
Explorer
Jan 19, 2026 12:39 PM UTC

low speed control can be difficult in some way but it depends how precise do you need to be on speed control. What is the requirement ?

HW/FW Motor Control Engineerhttps://www.linkedin.com/in/federicorodighiero/
geneMAuthor
Associate II
Jan 19, 2026 7:17 PM UTC

We're trying to get a 200:1 range of speed control. For example, the maximum speed of the motor may be 4000 RPM in which case the minimum speed will be 20 RPM.  The accuracy can be something like +/-5% although +/-10% may work. Velocity ripple should also be on the order of +/-5%.

Thanks for your interest.  I'll be happy to provide more details.

@GMA - I'm hoping you might be able to address my question of whether the ZeST or HSO algorithms provide any benefit in a low speed application with sensors.

 

federico.rodighiero87
Explorer
Jan 20, 2026 7:56 AM UTC

do you have a plot of the low speed issue ?

HW/FW Motor Control Engineerhttps://www.linkedin.com/in/federicorodighiero/
geneMAuthor
Associate II
Jan 20, 2026 3:13 PM UTC

We're just in the system design stage now.  I'm trying to figure out if we need to start with an eval board that supports ZeST or HSO or both like the ZeST discovery board.

GMA
ST Technical Moderator
Jan 20, 2026 4:41 PM UTC

Hello @geneM,

If a motor includes an encoder sensor, it is most effective to use the encoder for motor control.
HSO and STO-PLL algorithms are sensorless algorithms.

As motioned here, The STM32 ZeST algorithm is available for selected users only.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
geneMAuthor
Associate II
Jan 21, 2026 6:14 AM UTC

Hello @GMA 

 

Thanks for the quick response.  Just out of curiosity, how does ST select users for ZeST?  Also out of curiosity, will the ZeST algorithm provide any benefit for low speed control for a motor with an encoder?

Thanks

Gene Massion

GMA
ST Technical Moderator
Jan 21, 2026 3:51 PM UTC

Hello @geneM,

Refer to STM32 ZeST and HSO solutions page. 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA