Skip to main content
Visitor II
December 31, 2024
Question

L6480HTR Current problem

We are operating the motor with the Run command “Run(DIR, SPD)” to rotate it at a constant speed. However, when the speed (SPD) is varied and then returned to the same SPD, we observe a significant increase in current.

  • We send the Run command to the driver IC every 20ms.
  • Even when the motor status is constant speed “MOT_STATUS[1, 1]… Constant speed”, we continue to send the Run command. In this case, a slight speed variation causes the current to keep increasing.
  • When we tried not sending the Run command while the motor status was constant speed “MOT_STATUS[1, 1]… Constant speed”, the current change almost disappeared.

Therefore, could continuously sending the Run command while the motor status is “constant speed” affect the phase current adjustment in some way?

This topic has been closed for replies.