Question
L6470 Case Temperature Reached Thermal Warning
- 6 replies
- 1314 views
Hi ST expert,
I am experiencing stepper driver L6470 hot temperature issue and need your expert advice on my schematic design.
Symptom:
- During power-up --> No heat-up.
- After initialization --> Case temperature start to increase.
- Motor movement --> No issue.
My schematic as attached.
Input to the board is 48V step down to 36V using DC to DC converter.
Added current sense circuit at the input side of driver.
*Motor supply voltage compensation is disabled by FW.
Thank you so much in advance.