Skip to main content
Associate III
Jan 21, 2026 5:19 PM UTC
Solved

JSON file for a new motor to upload in Workbench?

Hello. I try to start a new project with two non-listed motors in Workbench. I use two gimbal 3-phase BLDC motor with encoder AS5048A https://cdn.sparkfun.com/assets/d/6/b/5/8/27477_27478_Datasheet.pdf Based on the motorShinano.json file, I built my own JSON file, please see below. However, I have the following questions. What to write in the compatibility: "sixStep"? The motor has the encoder. Hence, should TRUE be for HasHallSensor? I use a Pololu power board (voltage regulator) https://www.pololu.com/product/5576 and two Sparkfun 3-phase BLDC motor drivers https://www.sparkfun.com/sparkfun-brushless-motor-driver-3-phase-tmc6300.html . Therefore, what to write for pwr_board? What to write for foc_rate? What to write for acceleration and max_speed_startup? Thank you. 

{

"id": "motorSparkfun",

"label": "Sparkfun DM3505/3505EC",

"hardwareFamily": "MOTOR",

"description": "Outer rotor type - 11 poles pairs - brushless DC motor with encoder",

 

"compatibility": ["FOC", "sixStep"],

 

"polePairs": 11,

 

"nominalCurrent": 1.1,

"nominalDCVoltage": 12.0,

"rs": 6.34,

"ls": 1.08,

"magneticStructure": {

"type": "BLDC"

},

 

"BEmfConstant": 1.23,

"inertia": 56.0,

"friction": 0.04,

"maxRatedSpeed": 1610,

 

"hasHallSensor": true,

"hallSensor": {

"sensorsDisplacement": 120,

"placementElectricalAngle": 300

},

 

"hasQuadratureEncoder": true,

"quadratureEncoder": {

"pulsesPerMechanicalRevolution": 16384,

"hasIndexPin": false

},

 

"motorProfiler": {

"ctrl_board": "NUCLEO-F401RE",

"pwr_board": "???????????",

 

"operating_condition": {

"cutoff_frequency": 2000,

"pwm_frequency": 20000,

"foc_rate": ????

},

 

"mechanical": {

"acceleration": ?????,

"max_speed_startup": ?????

}

}

}

GMA
GMABest answer
ST Technical Moderator
Jan 26, 2026 8:31 AM UTC

Hello @Boris_L,

I made a mistake. You can remove hasHallSensor and hallSensor{}.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

3 replies

GMA
ST Technical Moderator
Jan 22, 2026 8:42 AM UTC

Hello @Boris_L,

If you want to select "FOC" or "sixStep" algorithm, "compatibility" is correctly set.
"motorProfiler{}" is not required, you can remove it.
The "hasQuadratureEncoder" and "quadratureEncoder{}" parameters can be removed if you do not have a quadrature encoder.
One point: For the "magneticStructure" type, use "SM-PMSM" or "I-PMSM".

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Boris_LAuthor
Associate III
Jan 23, 2026 6:26 PM UTC

Hello GMA,

I do not use Hall sensor. I use the encoder AS5048A. Can I remove the Hall section in my code? Thank you. 

GMA
GMABest answer
ST Technical Moderator
Jan 26, 2026 8:31 AM UTC

Hello @Boris_L,

I made a mistake. You can remove hasHallSensor and hallSensor{}.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA