Skip to main content
Associate III
November 14, 2024
Question

Issue in running motor using custom board STSPIN32F0

Dear,

 

I have custom board based on this https://github.com/issus/BLDC-Drive which uses STSPIN32F0 as motor driver. I have that got that PCB manufactured & assembled but stumbled on an issue (which I assume is an issue) that it does not have feedback resistors on current sensing op-amp circuits. I have added those manually on the PCB. I am able to program and connect to the board using MCSDK 5.4.8 monitor but whenever I press start motor start-up failure occurs.

 

I can share all the files need if required but I want to know the procedure to diagnose this startup issue. I have a 2-channel oscilloscope with me and I can probe those inverting signals as well.

 

MCSDK 5.4.8 & schematic are attached for your quick reference.

 

I will be grateful of your help in this matter.

 

Regards

Shahid

This topic has been closed for replies.

2 replies

GMA
ST Technical Moderator
November 14, 2024

Hello @x4ce,

As a first step, you can go through our FAQ page available here.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
x4ceAuthor
Associate III
November 14, 2024

Thank you

I will go through and get back to you.