Skip to main content
Liam G
Associate II
Apr 29, 2020 8:12 AM UTC
Question

Issue building EVALKIT-ROBOT1 project with Cube IDE on Mac.

Error links to an autogenerated file: subdir.mk with the below.

Any idea how to fix?

Project is set by default to generate makefiles automatically. Doesn't seem right for a project like this. Can't find a real makefile for CubeIDE in the provided project.

01:05:43 **** Incremental Build of configuration Debug for project EVALKIT_ROBOT_1_SDK543_Positioning_LL ****

make -j3 all 

Middlewares/modbus/rtu/subdir.mk:20: *** target pattern contains no '%'. Stop.

################################################################################

# Automatically-generated file. Do not edit!

################################################################################

# Add inputs and outputs from these tool invocations to the build variables 

C_SRCS += \

/Applications/STM32CubeIDE.app/Contents/MacOS/C:/workspace/MotorControl_SDK_Position\ Control\ Customization/FW/EVALKIT_ROBOT_1_SDK543_Positioning_LL/EVALKIT_ROBOT_1_SDK543_Positioning_LL/modbus/rtu/mbcrc.c \

/Applications/STM32CubeIDE.app/Contents/MacOS/C:/workspace/MotorControl_SDK_Position\ Control\ Customization/FW/EVALKIT_ROBOT_1_SDK543_Positioning_LL/EVALKIT_ROBOT_1_SDK543_Positioning_LL/modbus/rtu/mbrtu.c 

OBJS += \

./Middlewares/modbus/rtu/mbcrc.o \

./Middlewares/modbus/rtu/mbrtu.o 

C_DEPS += \

./Middlewares/modbus/rtu/mbcrc.d \

./Middlewares/modbus/rtu/mbrtu.d 

# Each subdirectory must supply rules for building sources it contributes

Middlewares/modbus/rtu/mbcrc.o: /Applications/STM32CubeIDE.app/Contents/MacOS/C:/workspace/MotorControl_SDK_Position\ Control\ Customization/FW/EVALKIT_ROBOT_1_SDK543_Positioning_LL/EVALKIT_ROBOT_1_SDK543_Positioning_LL/modbus/rtu/mbcrc.c

arm-none-eabi-gcc "$<" -mcpu=cortex-m0 -std=gnu11 -g3 -DARM_MATH_CM0 -DUSE_HAL_DRIVER -DSTM32F031x6 -DUSE_FULL_LL_DRIVER -DDEBUG -c -I../../Drivers/CMSIS/Include -I../../MCSDK_v5.4.3/MotorControl/MCSDK/MCLib/Any/Inc -I../../Drivers/STM32F0xx_HAL_Driver/Inc/Legacy -I../../MCSDK_v5.4.3/MotorControl/MCSDK/MCLib/F0xx/Inc -I../../Inc -I../../Drivers/CMSIS/Device/ST/STM32F0xx/Include -I../../MCSDK_v5.4.3/MotorControl/MCSDK/UILibrary/Inc -I../../MCSDK_v5.4.3/MotorControl/MCSDK/SystemDriveParams -I../../Drivers/STM32F0xx_HAL_Driver/Inc -I../../modbus/include -I../../modbus/rtu -I../../modbus/port -Os -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/modbus/rtu/mbcrc.d" -MT"$@" --specs=nano.specs -mfloat-abi=soft -mthumb -o "$@"

Middlewares/modbus/rtu/mbrtu.o: /Applications/STM32CubeIDE.app/Contents/MacOS/C:/workspace/MotorControl_SDK_Position\ Control\ Customization/FW/EVALKIT_ROBOT_1_SDK543_Positioning_LL/EVALKIT_ROBOT_1_SDK543_Positioning_LL/modbus/rtu/mbrtu.c

arm-none-eabi-gcc "$<" -mcpu=cortex-m0 -std=gnu11 -g3 -DARM_MATH_CM0 -DUSE_HAL_DRIVER -DSTM32F031x6 -DUSE_FULL_LL_DRIVER -DDEBUG -c -I../../Drivers/CMSIS/Include -I../../MCSDK_v5.4.3/MotorControl/MCSDK/MCLib/Any/Inc -I../../Drivers/STM32F0xx_HAL_Driver/Inc/Legacy -I../../MCSDK_v5.4.3/MotorControl/MCSDK/MCLib/F0xx/Inc -I../../Inc -I../../Drivers/CMSIS/Device/ST/STM32F0xx/Include -I../../MCSDK_v5.4.3/MotorControl/MCSDK/UILibrary/Inc -I../../MCSDK_v5.4.3/MotorControl/MCSDK/SystemDriveParams -I../../Drivers/STM32F0xx_HAL_Driver/Inc -I../../modbus/include -I../../modbus/rtu -I../../modbus/port -Os -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/modbus/rtu/mbrtu.d" -MT"$@" --specs=nano.specs -mfloat-abi=soft -mthumb -o "$@"

This topic has been closed for replies.

2 replies

KKuma.3
Associate
Jul 14, 2020 1:10 PM UTC

Hello @Liam G​  ,

However I was able to build the binary using Atollic true studio without any changes to the code.

Laurent Ca...
Senior III
Jun 15, 2021 7:46 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards