Skip to main content
ARuss.3
Visitor II
May 5, 2023
Question

Is the 3 Phase Inverter board "EVSPIN32F0601S1" capable of driving an AC Induction motor?

  • May 5, 2023
  • 1 reply
  • 943 views

Hello Everyone,

I am trying to control an AC Induction motor using the 3 Phase Inverter board "EVSPIN32F0601S1". According to the datasheet of the EVSPIN32F0601S1, it can control PMSM and BLDC motors. But, It didn't mention anything about the ACIM. My Questions are,

1) Is the 3 Phase Inverter board "EVSPIN32F0601S1" capable of driving an AC motor?

2) If so, Are there any available resources online?

This topic has been closed for replies.

1 reply

Gael A
ST Employee
September 4, 2023

Hello ARuss.3,

First of all, we would like to sincerely apologize for the delay in replying to your post.

Concerning your first question, the EVSPIN32F0601S1 should be able to run an AC motor, depending on its specification (just like any motor)

Concerning your second question, I am afraid that ACIM configurations are currently only available as examples on G4. If you want to use the F0, you need to adapt that code for your needs.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.