Skip to main content
Associate II
September 25, 2025
Solved

Is it possible to modify the B-G431B-ESC1 to achieve higher peak current?

  • September 25, 2025
  • 3 replies
  • 568 views

Hi Sir,

 

The peak current of the B-G431B-ESC1 is 40A. Is it possible to modify the board to achieve a higher peak current? If yes, what modifications would be required? If not, could you explain the limitations?

Thank you.

 

 
This topic has been closed for replies.
Best answer by STuser2

I assume it is mainly because of the PCB layout and copper thickness.   

3 replies

Senior III
September 25, 2025

To use the B-G431B-ESC1 board it needs to be cooled down, if you check the data sheet of the board on page6 

Output peak motor current (maximum peak current tested with a propeller to have an air-forced cooling): 40 A

 

TIENHUAAuthor
Associate II
September 25, 2025

Hi Sir,

 

Thank you for your reply. I have already reviewed the document you mentioned, where it states that the peak motor current of the B-G431B-ESC1 is 40 A with air-forced cooling.

Could you please help clarify what exactly limits the peak current to 40 A? For example, is this restriction mainly due to the PCB layout and copper thickness, the MOSFET thermal capability, the shunt resistor, or other design aspects?

I would like to better understand the design considerations behind this limitation.

STuser2Best answer
Senior III
September 25, 2025

I assume it is mainly because of the PCB layout and copper thickness.