Question
Is it possible to maintain torque when the motor's rotation speed is low (near 1000RPM)?
Hi, I am using NUCLEO-G431RB+X-NUCLEO-IHM16M1+MototControl Workbench 5.Y.3 to control a sensorless BLDC motor. The motor could maintain nice torque when rotation speed is above 10,000RPM~40,000RPM. However, when RPM was decreased to around 1000RPM, the motor will stop rotate when it touches a surface (i.e. any tiny friction could stop the motor) . Is it possible to maintain torque when the motor's rotation speed is pretty low (near 1000RPM?