Skip to main content
kkhli.1
Associate III
April 12, 2023
Question

implement a recurrent equation to servo and regulate the speed of the motor at a setpoint

I calculate the speed of a motor with the method input capture calbback() then I have the recurring equation of the motor control,U(k)=U(k-1)-0.04*e(k-1)+0.12*e (k)

e(k) error = reference speed - current speed

the problem that the command in the infinite loop changes even the engine stopped:

any suggestion please?

int PWM_PERIOD=100;

int pwmMin=0;

int resolution=10;

float speedMotor2;

float speedMotor1;

volatile float em1=0;

volatile float um1=0;

volatile float u1m1=0;

volatile float e1m1=0;

int tensionMax=19.5;

/* USER CODE END 0 */

volatile uint32_t IC1_Val1 = 0;

volatile uint32_t IC1_Val2 = 0;

volatile uint32_t IC2_Val1 = 0;

volatile uint32_t IC2_Val2 = 0;

volatile int Difference1 = 0;

volatile int   Difference2=0;

volatile int  Difference=0;

volatile int Is_First_Captured = 0;

volatile int Is_First_Captured1=0;

/* Measure Frequency */

volatile float frequency1 = 0;

volatile float frequency2 = 0;

int TIMCLOCK=50000000;

int PRESCALAR=50;

float firstTick=0;

float periodeMotor1=0;

void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)

{

if(htim->Instance==TIM2){

if(htim->Channel==HAL_TIM_ACTIVE_CHANNEL_1 && speedMotor1 ==0)

{

if (Is_First_Captured==0) // if the first rising edge is not captured

{

IC1_Val1 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1); // read the first value

Is_First_Captured = 1; // set the first captured as true

}

else  

          {

IC1_Val2 = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1); // read second value

if (IC1_Val2 > IC1_Val1)

{

Difference1 = IC1_Val2-IC1_Val1;

}

else if (IC1_Val1 > IC1_Val2)

{

Difference1 = (0xffff - IC1_Val1) + IC1_Val2;

}

float refClock = TIMCLOCK/(PRESCALAR);

frequency1 = refClock/Difference1;

speedMotor1 = (frequency2 * 60) / ( resolution);

Is_First_Captured = 0; // set it back to false

}

                           }

}}

uint16_t commande_to_pwm_value(float commande)

{

uint16_t pwm_value = (uint16_t)((commande / tensionMax) * PWM_PERIOD);

if (pwm_value > PWM_PERIOD)

{

  pwm_value = PWM_PERIOD;

}

if (pwm_value <0)

{

  pwm_value = pwmMin;

}

return pwm_value;

}

int main(void)

{

 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();

 MX_TIM1_Init();

 MX_TIM2_Init();

 /* USER CODE BEGIN 2 */

 TIM1->CCR1 = 100;

 HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);

 HAL_TIM_IC_Start_IT(&htim2,TIM_CHANNEL_1);

 while (1)

 {

 int vitesseRef=300;

 em1=(vitesseRef-speedMotor1);

 //commande m1

           um1=u1m1+0.1287*em1-0.0429*e1m1;

            u1m1=um1;

            e1m1=em1;

            float cm1=commande_to_pwm_value(um1);

            TIM2->CCR1=cm1;

   

}

}

This topic has been closed for replies.