Skip to main content
Visitor II
May 19, 2025 12:34 AM UTC
Question

IHM16M1 and G474RE

i am trying to use the IHM16M1 with the NUCLEO-G474RE.  i have it plugged into the top of the Nucleo board via the Morphio connectors.

I can supply power (12v) to the IHM16M1, but it does not seem to be powering the G474RE.

I have tried JP5 on the Nucleo in both E5V and 5V_VIN mode.

 

Am I missing something?  

The IHM07M1 works when connected this way, but I cant get the IHM16M1 to work.  

 

thanks.

This topic has been closed for replies.

1 reply

Gael A
ST Employee
May 19, 2025 8:17 AM UTC

Hello certified_prime,

The NUCLEO-G474RE can be supplied with power by 5 different means that can be found on the user manual UM2505 :

GaelA_0-1747641690059.png

When looking at the corresponding pins from the IHM16 schematics, there is apparently no connexion that can be made without adding an external wire (from CN7_18 to CN7_6 for example) :

GaelA_1-1747642389616.png

The layout is different for the IHM07, which explains why the power supply is directly provided.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.