Skip to main content
Visitor II
April 25, 2024
Question

IHM14A1

Hello,

I would try to use  the IHM14A1 shield  and  for now i only have a nucleo F2 series . it seemed in the document that this nucleo is not supported , can somebody tell me if it can't works  or maybe with some modifications on the example code.

 

thanks 

jerome

    This topic has been closed for replies.

    1 reply

    Cristiana SCARAMEL
    ST Employee
    May 6, 2024

    Hello @Jerome_DataP and welcome to the ST Community.

    From the hardware point of view you can use a Nucleo F2 series board to drive the X-NUCLEO-IHM14A1 shield.
    You can use generic GPIO to drive the motor driver expansion board.

    There are no libraries ready for this pair of boards, in fact the X-CUBE-SPN14 software is compatible with a selection of Nucleo board.

     

    "If you feel a post has answered your question, please click ""Accept as Solution"""