IHM08M1 with NUCLEO-H743ZI2 board in FOC mode.
Hi!
I need to control a BLDC motor in FOC mode. I have a NUCLEO-H743ZI and IHM08M1, I know that they are not compatible with the ST morpho connector. But I decided to connect them manually with wires.
On IHM08M1 board I removed capacitors C3, C5, C7, closed jumpers JP1&JP2, and soldered JP5&JP6 to 3Sh.
On Nucleo board I configured advanced TIM1 with 3 Channels:
TIM_CH1, TIM_CH1N,
TIM_CH2 TIM_CH2N,
TIM_CH3, TIM_CH3N
And wired them to the power board.
When I trying to generate PWM signal, there are any outgoing signal on any of 3 Phases.
Do I miss something?
Thank you!