Skip to main content
cchiau
Visitor II
July 31, 2016
Question

IHM07M1 ST workbench Motor Profile Overcurrent Fault

  • July 31, 2016
  • 1 reply
  • 613 views
Posted on July 31, 2016 at 20:13

Hi,

I have a the 

P-

NUCLEO

-IHM001 kit, and having issues completing the motor profile step.

Setup:

1. keil IDE loading firmware complete, board setup in FOC, 3 shunt jumpers.

2. ST workbench profile using example project ''P-Nucleo-IMH001-MP-LowInductanceMotor-7-PolesPairs''

3. generation location in SystemDriveParams folder

4. connectivity successful, after clicking ''start'' the motor starts to tick and move a little, goes through that part fine

3. sometimes it will spin up sometimes it won't, and that is the step where the over current fault occurs.

I've tried adjusting the ''Nominal Current'' in motor parameters, no change.

Power supply is steady and can produce up to 3A, 

Looking for assistance or pointers in where the current limit is set or resolution.  Much appreciated thank you

#foc-ihm07m1-motor-profiler
This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards