Skip to main content
freppa
Associate II
February 27, 2018
Question

ICS and F303?

Posted on February 27, 2018 at 10:19

In UM1052 it says that ICS current sensing is only available for F103 HD, F2xx, F4xx. However the class ICS_F30X_PWMnCurrFdbk is part of the MC Library. 

Is this class with it's functionality a work in progress? It does not compile as reported here:

https://community.st.com/message/174361-foc43-dual-motor-with-ics-sensors-and-stm32f3-does-not-compile

 

It seems that development of this class is started but not finished. But why include unfinished non-working SW in the lib? What is going on here?

I wish to run F303 single motor control with a 2-shunt inline current sense topology.  

#sw #ics #f303re
This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards