Skip to main content
JMust.1
Visitor II
October 22, 2021
Question

I will create code for discovery kit 'B-G431-ESC' as described in UM2516 chapter 6.1 step 2 and 3 but I get error when compiling with STM32CubeIDE . Is there a more detailed description for generation or an example for this evakit?

I use MCSDK v5.4.7 and STM32CubeIDE 1.6.1. Project generation with MCSDK is successful but when I try to build code with the IDE it ends with fatal error "sto_cordic_speed_pos_fdbk.h: No such file or directory". Run code generation with an other example project works well. So I asume that my tool chain is okay.

This topic has been closed for replies.

2 replies

ST Technical Moderator
October 22, 2021

Hello @JMust.1​ and welcome to the Community :)

I think you don't have the Include Paths set up coherently.

You have to review the defines and the include file paths for your project: Go to Project options ->C/C++ tab->Include paths and add new paths to your include directories.

Feel free to share your update and solution, It should be helpful for the Community =)

When your question is answered, please close this topic by choosing Select as Best.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate II
January 18, 2025

hi,

I have been trying to run PMSM motors with B-G431B-ESC1, I follow the steps given in the user manual,

1. I profile the motor and save the parameters

2. use the motor control workbench to generate a project, and generate source code,

3. run it in Cube IDE to flash it on the development board.

However, I am unable to run my motor with that source code. The motor doesn't even start. I also face inconsistency when running the motor with the same source code on different occasions. What could be the issue, and what should I do to resolve this issue?

since the profiler is working, where can I get a profiler code based on which the profiling .hex file is created to debug the issue?

Thank you,

Madhav