Skip to main content
LBara.1
Visitor II
December 21, 2020
Question

I downloaded the STSW-SPIN3204-V1.0.0 fw, and I can't import it into the STM32CubeIDE Version: 1.5.1.

Hi,

I inflated the en.stsw-spin3204.zip into the c:/PRG/STSW-SPIN3204-V1.0.0 directory.

I follow the UM3210 '2.5.2.3 Create a build with system workbench for STM32' but import was wrong. Maybe the fw source too old (2019.02.15) for new STM32CubeIDE? What can I do?  Do I import the files one-by-one by hand? :(

Ups! System Workbench.

The solution:

I have System Workbench on my computer, but I haven't used it in a long time. Import works with it, if I copy the files into the c:\GITshared\Cube\Stspin32f0_6steps_v1\stm32_cube\ directory.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 22, 2021

STM32 Motor Control topic added.

Best regards