Skip to main content
TYeo.1
Visitor II
March 26, 2020
Question

I can't get the STM32G431RB to run the program to get the motor working. How do I get the motor to run smoothly?

I have set the jumper pins with respect to the user manual.

The motor only runs after I profile it at the motor profiler, when I run the program into the board using the STM32CubeIDE, the motor stops running again. And when i want to profile it again it says that a firmware upgrade is needed for the board to connect to the profiler.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards