Skip to main content
This topic has been closed for replies.

3 replies

Cristiana SCARAMEL
ST Employee
January 31, 2023

Hello @SBrah.1​ and welcome to the ST Community.

Are you using the STM32 Motor Control Software Development Kit X-CUBE-MCSDK?

If so, what version?

Could you share more details on your application?

  • Single o three-shunt configuration
  • Sensored (Hall or encoder feedback) or sensorless (BEMF detection)

According to these hardware and firmware settings you can check the OC threshold set and verify if the over current protection is properly triggered by application.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Associate II
February 8, 2024

i have the same problem while using single shunt (sensorless) , motor pilot didn't even connect to the board

ABart.5
Associate II
April 26, 2023

Were you able to figure out the problem? I'm having the same issue.