Skip to main content
EOkum.1
Visitor II
June 12, 2023
Solved

I am getting this error when I try connecting my Hardware ( Nucleo-F302R8, IHM07 ) with STM Motor Profiler. What could be the issue?

..

This topic has been closed for replies.
Gael A
Gael ABest answer
ST Employee
June 19, 2023

Hello EOkum.1,

This issue is generally caused by hardware. Nevertheless, have you first tried choosing manually the two boards you are using via the "Select Board" button ?

If the problem persist, consider having a look at your board's jumpers, especially the CN2 jumpers on F302R8, which both need to be set. They allow ST-LINK for onboard programming, which is mandatory for profiler.

Please also keep in mind that profiling is only done on 3-Shunt configurations, and that your IHM07 needs to be configured that way, even though it should not impact ST-LINK connection.

Hoping this will help,
Gaël A.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

1 reply

Gael A
Gael ABest answer
ST Employee
June 19, 2023

Hello EOkum.1,

This issue is generally caused by hardware. Nevertheless, have you first tried choosing manually the two boards you are using via the "Select Board" button ?

If the problem persist, consider having a look at your board's jumpers, especially the CN2 jumpers on F302R8, which both need to be set. They allow ST-LINK for onboard programming, which is mandatory for profiler.

Please also keep in mind that profiling is only done on 3-Shunt configurations, and that your IHM07 needs to be configured that way, even though it should not impact ST-LINK connection.

Hoping this will help,
Gaël A.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.