Skip to main content
Aidan McCoy
Visitor II
June 3, 2018
Question

How to use Motor Profiler with STEVAL-ESC001V1

Posted on June 03, 2018 at 09:43

I am trying to use the STEVAL-ESC001V1 with the motor profiling tool but I can't get the motor profiler to connect to the controller. I am using a ST-LINK/V2 with the STSW-LINK009 driver on Win7. I am able to connect to the controller using the STM32 ST-LINK Utility so I think the wiring is correct and I am missing something on the motor profiler side of things. Any ideas on what the issue might be? I am getting 'Connection Error! Please, check the connection between the board and PC.'

This topic has been closed for replies.

2 replies

kyrreaa
Associate III
July 3, 2018
Posted on July 03, 2018 at 17:52

Correct. You also need a USB->serial adapter connected to the UART pins. They are unfortunately 1.27mm pitch so it's a bit fiddly.

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards