I am trying to evaluate STSPIN32F0251S1 ,
My requirement is use 6 steps ( trapezoidal ) implementation ,
I tried to use example project from motor control workbench 5.Y.4
[EVSPIN32F0251S1] + [Shinano LA052-080E3NL1] HW setup using
* the Six-Step algorithm Voltage modes and Sensorless
software packages
- STM32CubeMX v6.4.0
- STM32Cube_FW_F0_V1.11.2
when i tried update motor parameter and Generate code is show some error (image attached) .
if choose the only update option then code generates but motor parameter remain same.
Need some help