Skip to main content
Larry Lukis
Associate II
June 20, 2020
Question

How to use MC Workbench to generate project for STM32G474 in LQFP64 package?

I see that 128 pin package is supported even though it is a non-stocked item at Digikey. I can build a project for that package, but I need to build for the 64 pin package. How can I do that?

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards