Associate
Jul 9, 2024 4:56 AM UTC
Question
How to use demo kit???? (EVSPIN32G4 )
- 1 reply
- 1060 views
I used the Motor Profiler 5.4.8 program to extract the motor values of the 12v custom motor in picture 1 and created a project in MC_Workbench to operate it.
I bought an evspin32g4 board to test the operation of a larger voltage motor.
How can I extract the motor value using EVSPIN32G4?
There is no such board in the Motor Profiler 5.4.8 program.
I can create a project in the MC_Workbench program, but I do not have the corresponding motor, so please tell me how to proceed.