Skip to main content
Karan 123
Senior
May 15, 2020
Question

How to start with 3-Phase BLDC motor:

Hi,

I have to make low cost on BLDC for Industrial Sewing Machine with Three Hall Sensors and read about BLDC from resources available on internet .

I have P-NUCLEO-IHM001 for BLDC motor control

and seen below youtube video from ST.

https://www.youtube.com/watch?v=h3ZuM2Z0UGs

It's based on IAR workbench.

How to Start: ?

1) How to start with BLDC motor control application with STM32CubeIDE,CubeMX

with ST Motor profiler with P-NUCLEO-IHM001?

2) Is it possible to generate code for FOC or BLDC with Sensors (Hall) , Six Step Commutation etc. with Software Tool Chain ?

3) How to connect Customized Hardware MCU and Drive (MOSFET) board the STMotorProfiler?

4) As this board can operate motor the max rating of 1.4 A RMS. How to design hardware

driver circuit for with Six MOSFETs and Driver circuit compatible the Software Tool Chain ?

Any other suggestions ..

Thanks in Advance ..

--

Karan

--

Karan

This topic has been closed for replies.

12 replies

Claire O.
ST Employee
May 19, 2020

Hello Karan,

For your 3 first questions:

1/ Please use the MCSDK: https://www.st.com/en/embedded-software/x-cube-mcsdk.html

2/ Sensored FOC only is available for your slected board inside the MCSDK (not Six Step)

3/ Sorry the STMotorProfiler works only with ST boards so far...

Best regards,

Claire

Karan 123
Karan 123Author
Senior
May 19, 2020

Hi,

Thanks ..@ Claire OKU (ST Employee)

1) Will this board able to generate PWMs for Control operation of MOSFET for BLDC ?

2) How hall sensors are connected to this STM32 MCU?

 https://www.st.com/en/embedded-software/x-cube-mcsdk.html

0693W000001cYPoQAM.png

Thanks ..

--

Karan

Laurent Ca...
Senior III
October 14, 2020

Dear @Community member​ 

Do you have still these problems to solve?

Best regards

Laurent Ca...

Karan 123
Karan 123Author
Senior
October 15, 2020

Thanks...

​

Not Yet..

​

--

Karan​

Laurent Ca...
Senior III
October 15, 2020

Dear @Community member​ 

Therefore I consider this thread closed.

If need, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...

Karan 123
Karan 123Author
Senior
April 8, 2021

Hi,

Thanks.. Can I reopen now ? If yes ..

Please consider as below:

I have to make low cost on BLDC FAN without any Sensors and first rotate/spin BLDC Motor (70-110 VDC) then control speed of motor for Ceilling Fan Application ..

I already have P-NUCLEO-IHM001 board for 12V BLDC .

I have decided to buy (NRND Product ) for this application.

https://www.st.com/en/evaluation-tools/steval-ihm040v1.html

Because I want to use STM32F100C6T6B and  STGIPN3H60 in my application.

In this STEVAL-IHM040V1 hardware description Page 14 I have read "The BEMF sensing is not used by the FOC software".

Where Can I find demo code for that STSW-STM32100 ?

Can I use X-CUBE-MCSDK for generating Code of FOC to Rotate/SPIN the motor?

Any other suggestions are highly appreciated ...

--

Karan

Karan 123
Karan 123Author
Senior
April 8, 2021

Here is motor BLDC Motor Data:

110V DC , 32Watt , RPM 1350 Approx...

Karan 123
Karan 123Author
Senior
April 8, 2021

Hi,

I have also explored STEVAL-IHM038V1 (Active) for this application.

https://www.st.com/en/evaluation-tools/steval-ihm038v1.html

Where I can download demo code STSW-STM32100 (NRND) for that ?

--

Karan

MWeis.2
Visitor II
January 26, 2022

I am also looking for a research of an industrial sewing machine automation for my research paper. Can anyone help me out. Thanks

LPayn.1
Visitor II
January 29, 2022

Thanks for posting. Also looking for the same topic on industrial sewing machines for my M.S research

LPayn.1
Visitor II
January 30, 2022

Hopyfully my resarch paper on sewing embroidery machine automations will be published.