Skip to main content
omid hamdi
Associate III
Oct 19, 2019 11:50 PM UTC
Solved

HOW TO START MOTOR CONTROL FOC AC INDUCTION WITH STM32F

HI

ANY ONE KNOW HOW CAN START AC INDUCTION MOTOR WITH SDK5 LIBRARY OR ST HAVE LIBRARY FOR AC INDUCTION MOTOR

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:45 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

6 replies

NKale
Associate II
Dec 19, 2019 3:36 PM UTC

Hello Omid,

I am also looking for answer to this question. Do let me know if you got some pointers.

Thanks

Narendra

omid hamdi
Associate III
Dec 25, 2019 12:10 AM UTC

HI

OLD have ac with encoder v5 cannot support ac sensorless st plan in future add ac sensorless on library still cant support

if u need check ti website have more sample for ac induction bout if you need used st controller you must write program with your self

best regards

NKale
Associate II
Dec 25, 2019 4:27 AM UTC
Yes. Right now I am using TI processor (Tiva C series) but wanted to port same onto STM32 processor seems it is not possible at the moment.
Claire O.
ST Employee
Jan 17, 2020 1:36 PM UTC

Dear Omid and NKale,

We know the AC Induction motor control is missing in our library... Sorry about this! Anyway, the team keeps working to add day after days new features and SW. Please keep posted

Claire

Laurent Ca...
Senior III
Jun 15, 2021 8:07 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:45 PM UTC

Dear @omid hamdi​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards