Skip to main content
Associate
Aug 27, 2026 6:40 AM UTC
Question

How to solve the problem that the HSO is sensitive to the motor phase resistance

I have a motor whose phase resistance is 40 mΩ at 20 °C and 45 mΩ at 70 °C. When I set the phase‑resistance parameter to 40 mΩ, the motor operates normally at around 20 °C. However, when the motor temperature rises to approximately 50 °C, frequent start‑up failures occur. How can this problem be resolved?

3 replies

GMA
ST Technical Moderator
Aug 27, 2026 9:17 AM UTC

Hello ​@XGL,

Did you try selecting Start Up RsDC Estimation feature?

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
XGLAuthor
Associate
Aug 27, 2026 10:54 AM UTC

Thanks for your reply. I hadn’t enabled this feature. But if I turn it on, won’t errors in resistance identification impact the start‑up function?

XGLAuthor
Associate
Aug 27, 2026 10:57 AM UTC

Under the condition of the conventional STO observer, the influence of phase resistance appears to be minimal. From this perspective, the HSO seems less stable than the STO.