How to recreate example projects for Nucleo F302R8 + IHM07M1 hardware.
After running the profiler the demo example code is overwritten. I'd like to be able to create a project to duplicate the example code. I downloaded en.X-CUBE-SPN7.zip and tried to duplicate the F302R8 project by clicking on the STM32F302R8-Nucleo.ioc file in the CubeMx directory.
I get a warning to either migrate the project or to download the V1.8.0 firmware. If I migrate and build the code builds okay and downloads but there is no response from the motor. If I chose download the firmware the code builds without error but gives an error during debug that some commands can't be executed.
Are there any directions on how to build the example project for STM32CubeMX ?? Also, in my recreated project I don't see any calls to motor control apps in the code ?.
I've been frustrated on this for two weeks with no help from my distributor FAE or any contact from an ST FAE. It seems like reproducing a ST example project should be well documented somewhere.nvi
I found info indicating the SPN7 package has the project environment for IAR but I need a STM32CubeIDX project ....
Thanks for any and all help,