Skip to main content
DBohm.1
Associate
December 14, 2020
Question

How to migrate the CubeMX project (*.ioc file) to a different MCU

I have generated a Motor Control solution for CubeMX using MC Motor Workbench 5.4.4 and NUCLEO-G431RB and NUCLEO-IHM08M1 and successfully tested with my motor.

How can I to migrate the CubeMX project (*.ioc file) to a different MCU (STM32G431V(6-8-B)TX)?

This topic has been closed for replies.

7 replies

Laurent Ca...
Senior III
December 31, 2020

Dear @DBohm.1​ 

Sorry for the late answer.

Do you have still this problem to solve?

And just in case, if not, do not hesitate to share the final solution you found. Thanks by advance.

Best regards

Laurent Ca...

DBohm.1
DBohm.1Author
Associate
January 6, 2021

@Laurent Ca...​ 

Yes, I do still have the problem. I've hand edited the *.ioc file for motor control. Is there a better way?

Thanks,

Dave

Laurent Ca...
Senior III
March 11, 2021

Dear @DBohm.1​ 

For more readability, I move part of your question title in the question dscription.

Best regards

Laurent Ca...

Igor Cesko
ST Employee
March 17, 2021

Hello DBohm.1 ,

To port existing STM32CubeMX project to another microcontroller:

  • Create new STM32CubeMX project for target (new) microcontroller.
  • Then : File -> Import Project . And locate the existing project.
  • Conversion started with some warnings. Warnings shows some possible incompatibilities between MCUs and you can choose the solution.
  • Then please check the configuration of the new MCU and generate the code.
  • Use your files from old MCU project for implemented functionality.

I believe that you understand the functionality after first try.

Regards

Igor

THoll.4
Associate
November 17, 2021

This method currently doesn't work in V1.7.0. It skips the target selector screen and continues to the .ioc file selection screen. In any case, whatever I do it always import the MCU package related to the imported .ioc file and creates a new project. Please help, I need to migrate my code to three different chips within the stm32f4 series and re-configuring each project using the .ioc editor is a painfully tedious process.

Laurent Ca...
Senior III
June 21, 2021

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards