Skip to main content
Rkama
Visitor II
October 16, 2018
Question

How to integrate the parameters setup in MC workbench with IAR workbench for STEVAL-ESC001V1?

I am able to generate a IAR workbench workspace from MC workbench after setting all the parameters but I am stuck.I am generating a 490Hz PWM signal with 50% duty cycle but the motor doesn't rotate.Is it possible to change the PWM frequency in MC workbench? Am I making some other mistake?

This topic has been closed for replies.

2 replies

Giuseppe Scuderi
Associate II
April 5, 2019

Hi,

sorry for this huge delay.

Do you have solved the issue mentioned ? Please upgrade the SW with X-CUBE-MCSDK and for PWM management please visit the section " Drone Zone" in this forum.

BR

Giuseppe Scuderi

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards