Skip to main content
Abdul Fourteia
Associate II
Apr 18, 2018 11:51 PM UTC
Solved

How to install stm32 motor control workbench

Posted on April 19, 2018 at 01:51

Hello,

I recently bought two BLDC motor controllers, the STEVAL-SPIN3202 and the X-NUCLEO-IHM08M1 shield forNUCLEO-F401RE.

I have a project to control a BLDC sensored motor. I am not sure how to move forward. I have AC6, IAR and MKD installed. I have tried installed motor control workbench with no luck. X-CUBE-MCSDK executable that can be downloaded from the following link does not work for some reason.

http://www.st.com/en/embedded-software/stsw-stm32100.html

 

I am wondering if there is something else I need to install for this to work?

FIY, I am using Windows10 and I have STM32CubeMX installed.

This topic has been closed for replies.
cedric h1
cedric h1Best answer
Visitor II
Apr 19, 2018 7:46 AM UTC
Posted on April 19, 2018 at 09:46

It seems that the X-CUBE-MCSDK package is actually a zip file and not an exe. 

If Windows complains that 'The version of this file is not compatible with the version of windows you're running' Try to unzip the file first. It should be fixed in the coming hours...

If you agree with my answer, please accept it by clicking on 'Accept as solution'.""

10 replies

cedric h1
cedric h1Best answer
Visitor II
Apr 19, 2018 7:46 AM UTC
Posted on April 19, 2018 at 09:46

It seems that the X-CUBE-MCSDK package is actually a zip file and not an exe. 

If Windows complains that 'The version of this file is not compatible with the version of windows you're running' Try to unzip the file first. It should be fixed in the coming hours...

If you agree with my answer, please accept it by clicking on 'Accept as solution'.""
Abdul Fourteia
Associate II
Apr 19, 2018 10:19 PM UTC
Posted on April 19, 2018 at 22:19

Thank you for your help.

You are correct. I changed the file domain to zip, and when I unzipped it, another executable showed up. I was able to run that, and it seems the problem is fixed on the server side as well.
gokay aygok
Associate III
Apr 20, 2018 4:06 PM UTC
Posted on April 20, 2018 at 18:06

hi Abdul,

Have you succeed in installing and generating the code for motor control ? 

Abdul Fourteia
Associate II
Apr 21, 2018 5:29 AM UTC
Posted on April 21, 2018 at 05:29

Yes, I managed to install it, but I haven't tried it out yet.

gokay aygok
Associate III
Apr 21, 2018 8:35 AM UTC
Posted on April 21, 2018 at 08:35

Thanks

Could you me please let me know if code generation is successfully working ? I am fed of trying to generate code, but I having some problems in generating the code. (with mcsdk 5.0.2 or 5.0.3)

thanks a lot Abdul...

Laurent Ca...
Senior III
Jun 28, 2021 1:28 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards