Skip to main content
llantalan .
Associate II
November 9, 2017
Question

How to I remove the initial high speed ramp up of the motor on the potentiometer example?

Posted on November 10, 2017 at 00:23

When running the potetiometer example on the ST motor control workbench, there is an initial ramp up before it settles to the value based on the ADC reading of the potentiometer. Is there a way to remove this so that it always follows the potentiometer?

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards