Skip to main content
CPrin
Associate II
March 26, 2019
Question

How to get one PWM output inverted?

I have the Shinano motor running correctly with the NUCLEO-F303RE board and the X-NUCLEO-IHM08M1. 

I'm trying now to get it working with our custom board. Unfortunately my hardware colleagues have used the NCP5304 bridge driver instead of the L6398 driver. The NCP5304 has a smitt-trigger inverter on both IN-Hi and IN-Lo inputs where the L6398 has only an inverter at the IN-Lo (LIN) input. The PWM signal to the bridge driver shows now identical signals at both inputs, which is correct for the L6398 driver. But for the NCP5304 I need one PWM signal to be inverted. Can this be done easily? I tried to do that with the MCWB by changing the "Power Stage - Driving Signals Polarity" but this seems not to be working.

This topic has been closed for replies.

3 replies

Uwe Bonnes
Chief
March 26, 2019

Look at the CCxP and CCXNP bits in CCER.

CPrin
CPrinAuthor
Associate II
April 8, 2019

Thanks for your reply Uwe! You are right, that helped. Finally I found, that I could achieve the same by setting the "Power Stage - Driving Signals Polarity of both driving signals (High side & Low side) both to "Active Low" and this results in having one PWM output to be inverted. The "complemented from high side" box has to be "unchecked". It seems on first sight illogical but actually it is logical.

Laurent Ca...
Senior III
June 28, 2021

Adding of "STM32 Motor Control" topic.

Best regards.