Skip to main content
Jim Frederick_2
Associate II
April 2, 2018
Question

How to generate project code for STEVAL-SPIN3202?

Posted on April 02, 2018 at 20:57

I'm attempting to generate project code for the STEVAL-SPIN3202.

ST32CubeMX doesn't have an option for the 

STEVAL-SPIN3202 so I tried using the ST Motor Control Workbench and it gives an error 'STSPIN mcu not supported in the FW for SDK5'.

Meanwhile, I'm using the example project provided in 'STSW-SPIN3202'.

Is there an add-on for ST32CubeMX to generate code for the 

STEVAL-SPIN3202?

Should the ST Motor Control Workbench generate code for the

STEVAL-SPIN3202?

Is the STEVAL-SPIN3202 and older product and maybe I'd find better support for a newer variant?

This topic has been closed for replies.

9 replies

Vitaliy Chernobay
Senior
April 9, 2018
Posted on April 09, 2018 at 17:59

STSPIN32F0A include STM32F031 

http://www.st.com/resource/en/datasheet/stspin32f0a.pdf

 
Jim Frederick_2
Associate II
April 13, 2018

Posted on April 13, 2018 at 14:46

Since the

STEVAL-SPIN3202 isn't supported by the current STMCWB 5.0, I abandoned it and switched to a board combination that is supported: a NUCLEO-F302R8 and X-NUCLEO-IHM08M1 motor controller board.

Found a similar question here

https://community.st.com/0D50X00009XkWsFSAV

with a file

<LINK NO LONGER ACTIVE>

Vitaliy Chernobay
Senior
April 14, 2018
Posted on April 14, 2018 at 11:46

0690X0000060AacQAE.png

look at the last line

Jim Frederick_2
Associate II
April 14, 2018
Posted on April 14, 2018 at 19:39

Vitaliy-

Good point but I still got the 

error '

STSPIN mcu not supported in the FW for SDK5

'. I'll try opening that SPIN3201 project and try it with the SPIN3202. I'll post a question asking what the difference is between a 3201 and 3202. 

BTW, your post with the PDF - were you trying to say RTFM? I'm not sure what your point was. I already had, and read, that PDF but it didn't really help with the STMCWB. I wasn't sure if you were suggesting that I skip the software tools and just write code from scratch - which certainly is another valid way of approaching the problem.

-Jim

Dale Spanheimer
Visitor II
April 14, 2018
Posted on April 14, 2018 at 05:13

So far, I have been completely disgusted with how great the advertising makes the STSPIN32F0 and STSPIN320A sound as well as the STEVAL-PIN3202, but how much a disaster the actual available support examples are. The description says it fully supports the STSW-TM32100 FOC software development kit, but trying to use it with that sdk has only lead to complete frustration and a substantial reduction in desire to use ST products of any kind. Everything I try ends up as a waste of time and money that does not work right. I really used to have a much higher opinion of ST, but my faith is shrinking with each disappointment.

Jim Frederick_2
Associate II
April 14, 2018
Posted on April 14, 2018 at 19:45

Dale-

You're confirming my suspicions that the SPIN stuff is being sidelined. I figured if that was really true that there'd be more chatter on the internet - or a roadmap. I was puzzled by the silence and lack of response. So far, I'm making much more progress with the 

NUCLEO-F302R8 and X-NUCLEO-IHM08M1 and FOC combination. I'm writing code on the PC side to talk to the FW using the motor-control protocol. Now why isn't that already available somewhere.

-Jim

cedric h1
Visitor II
April 18, 2018
Posted on April 18, 2018 at 18:38

Dear Jim,

STEVAL-SPIN3202, 

STEVAL-SPIN3201 will be back in the 5.1 release scheduled for end of May.

As the SPIN32F0 is based on a STM32F03 MCU, you can already generate the code with the 5.0.3 release but it is not so straightforward. 

Regrads

Cedric

If you agree with my answer, please accept it by clicking on 'Accept as solution'.""
Jim Frederick_2
Associate II
April 19, 2018
Posted on April 19, 2018 at 16:22

Cedric-

Thank you for the info. I'll revisit this in May/June. 

-Jim

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards