Skip to main content
c1ron
Associate II
May 3, 2022
Question

How to fix the "ASPEP_RESP ERROR:ERROR_NO_TXSYNC_SPACE" error in the ST Motor Pilot V.0.9.7

The error is for the UART communication between the STM32F303 control board and the ST Motor Pilot software, but what does it mean exactly ? Where can I find information about such errors ? My best guess is that there is a problem with a buffer for the UART, but is the problem due to my PC ? Is the baud rate to high ? Is it due to using the high frequency plot feature in the Motor Pilot software ?

This topic has been closed for replies.

1 reply

MKara.14
Visitor II
June 15, 2022

Hi I'm having the same problem, did you solve the problem? if you solved the problem, can you help me ?