Skip to main content
BTrem.1
Senior
January 19, 2021
Question

How to disable ST MCSDK DAC use in generated project code?

Background:

I'm trying to set up DAC1 Ch1 & Ch2 on my motor project and need some understanding of the DAC use. I have read the Ref Manual but am still struggling.

My motor project is using a STM32G431C8Ux (48-pin) device but MCSDK does not offer this as an option so I made a MCSDK project with a STM32G431CBUx device and generated a *.STMX file and *.ioc file. I then created a new *.ioc file for the STM32G431C8Ux by importing data from the first project. This approach was suggested by an ST Field Engr.

This seems to be working and I can spin the motor.

Problem:

My problem is I want to use DAC1 Ch2 to output data for another use. Apparently in my MCSDK project both channels of DAC1 were setup to output data. This has rendered my DAC1_CH2 as not usable. I'm trying to find where in the *.STMX file or *.ico file does it set up the DACs to be used for the ST debug channels. I want to disable the use of DAC1_CH2 by the ST motor code so I can use it in my code.

Presently, this is my Mx_DAC1_Init code:

static void MX_DAC1_Init(void)
{
 /* USER CODE BEGIN DAC1_Init 0 */
 /* USER CODE END DAC1_Init 0 */
 DAC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN DAC1_Init 1 */
 /* USER CODE END DAC1_Init 1 */
 /** DAC Initialization
 */
 hdac1.Instance = DAC1;
 if (HAL_DAC_Init(&hdac1) != HAL_OK)
 {
 Error_Handler();
 }
 /** DAC channel OUT1 config
 */
 sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_AUTOMATIC;
 sConfig.DAC_DMADoubleDataMode = DISABLE;
 sConfig.DAC_SignedFormat = DISABLE;
 sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
 sConfig.DAC_Trigger = DAC_TRIGGER_SOFTWARE;
 sConfig.DAC_Trigger2 = DAC_TRIGGER_NONE;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_EXTERNAL;
 sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /** DAC channel OUT2 config
 */
 sConfig.DAC_Trigger = DAC_TRIGGER_SOFTWARE;
 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_EXTERNAL;
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DAC1_Init 2 */
 /* USER CODE END DAC1_Init 2 */
}

I am using DAC1_CH2 in my own code as shown below. Even if I make y0 a constant 2047, the output is a sinewave that follows the motor bemf. The data appears to be a combination of my write and the ST debug write.

/* y0 is filtered bemf */
	y0 = FilterBEMF( x0 );
	
	/* write to DAC to observe during debug .... still spiky ? ---.... */
	DAC1->DHR12R2 = y0;
	DAC1->SWTRIGR = DAC_SWTRIGR_SWTRIG2;

Thanks,

edit Additional Info:

In file stm32g4xx_mc_it.c I modified the code as shown below:

 before:
// Highfrequency task
 UI_DACUpdate(TSK_HighFrequencyTask());
 /* USER CODE BEGIN HighFreq */
 
after:
 TSK_HighFrequencyTask();

This is not a permanent fix, for one, it is not in USER code. But, It did disable the DAC1 update except for the update I do in my code. This works and I see the sinewave I am generating and there are no 'spikes'.

Tis just shows the MCSDK update of the DAC1 CH1 and CH2 is the source of my problem. Where do I enable/disable this function in the generated C code?

This topic has been closed for replies.

3 replies

Dario CUCCHI
ST Employee
February 9, 2021

Hi @BTrem.1​ ,

Have you already tried to disable the DAC in the MCSDK project ?

Select the "DAC Functionality" block and select "Not Used" for both DAC channels.

0693W000007EYs3QAG.pngThen generate the .ioc and proceed as you already have described.

In the C source code you can add the configuration of the DAC as you need.

I hope this can help you !

BTrem.1
BTrem.1Author
Senior
February 16, 2021

I haven't tried this yet but plan to do so. I've been hesitant to try because I didn't want the code regeneration to replace any code I need in my existing project. I'll try this on a backup directory then do a 'Beyond Compare' folder comparison on the result with my existing project.

Thanks,

BT

Laurent Ca...
Senior III
June 1, 2021

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 SDK). 

Best regards

Laurent Ca...